Add a project using Project Setup
Project Setup lets you quickly set up a Power Operation project. Using Project Setup, you can:
- Create and name a project
- Select screen resolution and contrast
- Specify primary and secondary server connections
- Specify the Advanced Reports and Dashboards connection
- Add users and link user roles to Windows authentication
- Add devices to a project
- Add default pages
- Add runtime menus
- Choose the landing page for each monitor in a multi-monitor project
After you create the project and define its features, you can also use Project Setup to change other settings, such as devices in the CSV file, and to update your project.
For a list of project-related parameters that are created using Project Setup, see Project Setup – Changed Parameters.