Menus and Display Pages
Use Menus and Display Pages to add top-level menus that display in the runtime human-machine interface (HMI). The HMI is the view that users see. You can also define the default runtime page that will display on a monitor.
To add menus and landing pages:
- Under HMI Menus, select the top-level menu items that you want to include in the HMI.
NOTE: You can add more menu levels in the Power Operation Studio Menu Configuration page: Visualization > Menu Configuration.
- (Optional) If you have multiple monitors in your system:
- Under Monitors, enter the number (up to 8) of monitors in the Total Monitors field. You can also select the plus and minus buttons to increase or reduce the number.
- Under Runtime Landing Page, the corresponding number of monitors are enabled.
- For each monitor, select landing page you want to see when this monitor views Power Operation
- Select Next.
For more information on Power Operation menu configuration, see Power Operation Runtime menus.