FFT Module
The FFT Module performs Fast Fourier Transforms on waveforms sampled by the Data Acquisition Module.
Module icon
Overview
This module prepares the waveforms for input into other harmonics analysis and measurement modules.
NOTE: The registers and settings available in this module depend on the device or node you are configuring, as well as its firmware and template versions. Not all registers or settings are available on all devices or the Virtual Processor, and labels may vary.
Inputs
Source
The Source inputs to each FFT Module are factory-linked to the outputs of the Data Acquisition Module, and cannot be changed.
Enable
The Enable input is factory-linked and cannot be altered.
Setup registers
The FFT Module has no setup registers.
Output registers
FFT
The output FFTs can be linked to the following modules: Harmonics Analyzer, Harmonics Evaluation, Harmonics Measurement, Mains Signaling Evaluation, Power Harmonics, Symmetrical Components, Transient and Waveform Recorder.
Event
All events produced by the module are written into this register.
Possible events and their associated priority numbers are shown in the following table:
| Event priority group | Priority | Description |
|---|---|---|
| Setup Change | 10 | Input Links, setup registers or labels have been changed. |
The Event output register stores the following information for each ION event: time stamp, priority, cause, effect, and any values or conditions associated with the cause and effect.
Responses to special conditions
The following table summarizes how the FFT Module behaves under different conditions:
| Condition | Response of output registers |
|---|---|
| If the inputs are not available | The output registers are not available. |
| When the device is started or powered-up (either the first time, or after a shut-down) | The output registers are not available. |