Power Quality Aggregator Module

The Power Quality Aggregator module outputs the following power quality parameters: voltage aggregates, current aggregates, voltage over and under deviation aggregates, sliding reference voltage and power frequency.

Module icon

Overview

The Power Quality Aggregator module has pulse outputs for the IEC 61000-4-30 Class A compliance (“4-30”) intervals (150/180 cycles, 10 seconds, 10 minutes and 2 hours).

Note: Use the pulse outputs of the Power Quality Aggregator module (not a Periodic Timer module) to trigger downstream modules such as Data Recorder modules in order to help preserve aggregate data integrity.

Note: The registers and settings available in this module depend on the device or node you are configuring, as well as its firmware and template versions. Not all registers or settings are available on all devices or the Virtual Processor, and labels may vary.

The Power Quality Aggregator Module complies with the following sections of the IEC 61000-4-30 standard:

  • r.m.s. voltage refreshed each half-cycle, Urms (1/2)
  • Measurement aggregation over time intervals
  • Measurement aggregation algorithm
  • Power frequency
  • Magnitude of the supply voltage
  • Calculation of a sliding reference voltage
  • Underdeviation and overdeviation
  • Magnitude of current

For more information on IEC 61000-4-30 implementation in ION meters, refer to the IEC 61000-4-30 Compliance and ION meters technical note.

Inputs

The Power Quality Aggregator Module has the following inputs:

VLN1, VLN2 and VLN3

These registers are linked to the Vln a, Vln b, and Vln c outputs of the High Speed Power Meter module and cannot be changed.

VLL12, VLL23 and VLL31

These registers are linked to the Vll ab, Vll bc, and Vll ca outputs of the High Speed Power Meter module and cannot be changed.

VoltsMode

This register reflects the power system's configuration. This register is linked to the Volts Mode setup register on the High Speed Power Meter module and cannot be changed. The VoltsMode determines which High Speed Power Meter module outputs (line-to-neutral or line-to-line) are used to calculate the outputs of the Power Quality Aggregator module. The table below shows what Power Quality Aggregator inputs are used for the 3 voltage aggregates based on the different VoltsMode settings.

VoltsMode register setting Input link to High-Speed Power Meter
V1 aggregate V2 aggregate V3 aggregate
4W-Wye or 9S ‑ 4 Wire Wye/Delta V LN1 to Vln a V LN2 to Vln b V LN3 to Vln c
3W-Wye or 29S ‑ 4 Wire Wye or 36S ‑ 4 Wire Wye V LN1 to Vln a V LN2 to Vln b V LN3 to Vln c
Delta or 35S ‑ 3 Wire V LL12 to Vll ab V LL23 to Vll bc V LL31 to Vll ca
Single V LN1 to Vln a V LN2 to Vln b N/A
Demo N/A N/A N/A

Line-to-line (LL) values are used for systems that do not have a neutral. Line-to-neutral (LN) values are used for systems with a neutral. You can override this behavior with the Volts Method setup register.

NomVolts

This register specifies the nominal voltage of the power system.

I1, I2 and I3

These registers are linked to the High Speed Power Meter module’s I a, I b and I c outputs respectively and cannot be changed.

NomFreq

This register is linked to the NomFreq setup register of the Factory module and cannot be changed.

Enable

This register enables or disables the module. Linking this input is optional; if you leave it unlinked, the module is enabled by default.

Setup registers

Volts Method

This register determines the input values used by the Power Quality Aggregator module. When volts mode v ll is selected, the module uses the VLL inputs to calculate all V outputs with an unstated configuration. In automatic - pm volts mode dependent, the module uses either V1, V2 and V3 inputs or the V1 Delta, V2 Delta and V3 Delta inputs for its calculations, based on the Volts Mode setting in the Power Meter module. Any VLL or VLN labeled outputs are unaffected.

Output registers

The Power Quality Aggregator module contains the following output registers:

V1 150 180 Cycle (V1 3s), V2 150 180 Cycle (V2 3s), and V3 150 180 Cycle (V3 3s)

These registers are the 150/180 cycle measurements for magnitude of supply voltage as described in 4-30 section 4.4. The output values are updated at the completion of each 150/180 cycle interval.

Note: V3 150 180 Cycle (V3 3s) is set to n/a when VoltsMode is set to single.

I1 150 180 Cycle (I1 3s), I2 150 180 Cycle (I2 3s), and I3 150 180 Cycle (I3 3s)

These registers are used in the 150/180 cycle measurement for current, as described in 4-30 section 4.4. The output values are updated at the completion of each 150/180 cycle interval.

V1, V2 and V3 OverDev 150 180 Cycles

These registers are the overdeviation 150/180 cycle aggregates based on the 10/12 cycle overdeviation aggregates, as described in 4-30 section 5.12. The output values are updated at the completion of each 150/180 cycle interval.

V1, V2 and V3 UnderDev 150 180 Cycles

These registers are the underdeviation calculations based on the 10/12 cycle underdeviation aggregates, as described in 4-30 section 5.12. The output values are updated at the completion of each 150/180 cycle interval.

150 180 Cycle Pulse

This register is pulsed at the end of 150/180 cycle intervals.

V1 10 Minute, V2 10 Minute, and V3 10 Minute

These registers are the 10 minute interval aggregates of the basic measurement intervals (10/12-cycle) described in 4-30 section 4.4. The values are updated every 10 minutes.

I1 10 Minute, I2 10 Minute, and I3 10 Minute

These registers are the 10 minute interval aggregates of the basic measurement intervals (10/12-cycle) described in 4-30 section 4.4. The values are updated every 10 minutes.

Note: I3 10 Minute is set to n/a when VoltsMode is set to “single”.

Note: For the voltage and current 10 minute interval aggregates, if the 10 minute interval ends during a 10/12 cycle, the values will not update until the 10/12 cycle is completed. Therefore the interval may be 10 minutes plus up to one 10/12 cycle in length, as specified by the 4-30 Class A aggregation requirements.

V1, V2 and V3 OverDev 10 Minute

These registers are the overdeviation calculations based on the 10 minute Vrms as described in 4-30 section 5.12. The values are updated every 10 minutes.

V1, V2 and V3 UnderDev 10 Minute

These registers are the underdeviation calculations based on the 10 minute Vrms as described in 4-30 section 5.12. The values are updated every 10 minutes.

10 Minute Interval Pulse

This register is pulsed at the end of every 10 minute aggregation interval.

2 Hour Interval Pulse

This register is pulsed at the end of every 2 hour aggregation interval.

Power Frequency

This register is the ratio of the number of integral cycles counted during a 10 second clock interval, divided by the cumulative duration of the integer cycles. Individual cycles that overlap the 10 second boundary are discarded from the measurement as defined in 4-30 section 5.1.

Power Frequency Channel

This numeric register is the internal channel number where frequency is being measured.

Power Frequency Update

This register is pulsed when the Power Frequency has been updated, pulsed at approximately 10 second intervals synchronized to the clock.

VLN1 Half-Cycle, VLN2 Half-Cycle, VLN3 Half-Cycle

These registers are the LN rms voltages measured over 1 cycle, commencing at a fundamental zero crossing, and refreshed every half-cycle as defined in 4-30 section 3.24.

VLL12 Half-Cycle, VLL23 Half-Cycle, VLL31 Half-Cycle

These are the L-L rms voltages measured over 1 cycle, commencing at a fundamental zero crossing, and refreshed every half-cycle as defined in 4-30 section 3.24.

Sliding Reference Voltage

This is calculated using the aggregate of V L1-N or V L1-L2, depending on the VoltsMode, as defined in 4-30 section 5.4.4.

V1 Sliding Ref Voltage

This register contains the sliding reference voltage for V1, as defined in 4-30 section 5.4.4.

V2 Sliding Ref Voltage

This register contains the sliding reference voltage for V2, as defined in 4-30 section 5.4.4.

V3 Sliding Ref Voltage

This register contains the sliding reference voltage for V3, as defined in 4-30 section 5.4.4.

Vavg Sliding Ref Voltage

This register contains the average sliding reference voltage for all three phases (V1, V2 and V3), as defined in 4-30 section 5.4.4.

Event

All events are recorded in the Event register.

Possible events and their associated priority numbers are:

Event priority groupPriorityDescription
Setup Change10Input links, setup registers or labels have been changed

The Event output register stores the following information for each ION event: time stamp, priority, cause, effect, and any values or conditions associated with the cause and effect.