Safety precautions
Installation, wiring, testing and service must be performed in accordance with all local and national electrical codes.
danger
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
● | Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E in the USA, CSA Z462 or applicable local standards. |
● | Turn off all power supplying this device and the equipment in which it is installed before working on the device or equipment. |
● | Always use a properly rated voltage-sensing device to confirm that all power is off. |
● | Do not use the data from the meter to confirm the power is off. |
● | Replace all devices, doors and covers before turning on power to this equipment. |
● | Incorrectly configured ION modules may render the meter non-functional. Do not modify a module’s configuration without understanding the impact to the meter and any associated devices. |
Failure to follow these instructions will result in death or serious injury.
warning
unintended operation
Do not use this device for critical control or protection applications where human or equipment safety relies on the operation of the control circuit.
Failure to follow these instructions can result in death, serious injury, or equipment damage.