FUNCTION CanReconfigure : BOOL
The function returns TRUE if itfNode can perform a Reconfigure-Action. Only nodes implementing IReconfigureProvider can be used as input of Reconfigure
InOut:
Scope |
Name |
Type |
Return |
CanReconfigure |
BOOL |
Input |
itfNode |