TYPE ERROR :
This enumeration describes errors which may occur when working with the functions of this library.
InOut:
Name |
Initial |
Comment |
0 |
no error |
|
1300 |
first library-specific error |
|
1301 |
Timeout occured. |
|
1302 |
Operation was aborted. |
|
1303 |
The interface reference was invalid. |
|
1304 |
The function is not supported. |
|
1305 |
A general I/O configuration error occured. |
|
1306 |
Invalid parameter. |
|
1307 |
The specified node does not exist. |
|
1308 |
Dynamic memory allocation is disabled or system is out of memory. |
|
1309 |
The specified I/O address is not valid. |
|
1310 |
There is no associated IDevice instance for the specified I/O address. |
|
1311 |
There is no data available. |
|
1312 |
Operation not possible due to the current state |
|
1350 |
first manufacturer-specific error |
|
1399 |
last error |