PROC_STATE (ENUM)

 

TYPE PROC_STATE :

This enumeration is used to issue the current operation state of asyn­chronous methods.

InOut:

Name

Initial

Comment

DORMAND

0

The operation is in IDLE state.

BUSY

The operation is busy.

DONE

The operation is done.

ABORTED

The operation has been aborted.

ERROR

An error occured.