TYPE IEC_CYCLE_STRUCT : STRUCT
This struct is passed as parameter to the TaskEntryFunction, see IecTaskCreate
InOut:
Name |
Type |
pTaskInfo |
POINTER TO Task_Info2 |
pApplication |
POINTER TO APPLICATION |
hTaskHandle |
RTS_IEC_HANDLE |
bResult |
BOOL |
bDummy1 |
BOOL |