IecTaskDisableScheduling (FUN)
FUNCTION IecTaskDisableScheduling : RTS_IEC_RESULT
Disable scheduling for the specified task
InOut:
Scope |
Name |
Type |
Comment |
Return |
IecTaskDisableScheduling |
RTS_IEC_RESULT |
Returns the runtime system error code (see CmpErrors.library) |
Input |
hIecTask |
RTS_IEC_HANDLE |
Handle of the task |