FUNCTION IecTaskEnableWatchdog : RTS_IEC_RESULT
Enable watchdog for the specified task
Note
You have to disable the watchdog of the task before with IecTaskDisableWatchdog and _not_ with IecTaskDisableWatchdog2, because they act on different task flags!
The watchdog is enabled only at the next IEC cycle and _not_ immediately after calling this function!
If you disable with IecTaskDisableWatchdog and forgot to enable it, at least at the next cycle, the watchdog is automatically enabled!
InOut:
|
Scope |
Name |
Type |
Comment |
|
Return |
IecTaskEnableWatchdog |
RTS_IEC_RESULT |
Returns the runtime system error code (see CmpErrors.library)
|
|
Input |
hIecTask |
RTS_IEC_HANDLE |
Handle of the task |