FUNCTION IecTaskGetCurrent : RTS_IEC_HANDLE
Funktion to get own task handle
InOut:
Scope |
Name |
Type |
Comment |
Return |
IecTaskGetCurrent |
RTS_IEC_HANDLE |
Returns the current IEC task handle |
Input |
pResult |
POINTER TO RTS_IEC_RESULT |
Pointer that returns the runtime system error code (see CmpErrors.library) |