FUNCTION IecTaskReload : RTS_IEC_HANDLE
Reload a specified IEC task. Reload means here: Delete the task at the actual position and create it newly.
InOut:
|
Scope |
Name |
Type |
Comment |
|
Return |
IecTaskReload |
RTS_IEC_HANDLE |
Handle to the new created task |
|
Input |
hIecTask |
RTS_IEC_HANDLE |
Handle to the task to reload |
|
udiTimeoutMs |
UDINT |
Timeout in milliseconds to wait, until the task deleted itself. Timeout can be one of the following predefined values:
See Timeouts details. |
|
|
pResult |
POINTER TO RTS_IEC_RESULT |
Pointer to error code |