TYPE DP_DIAG : STRUCT
Data structure containing DP Slave diagnosis data (see: RDIAG).
(see IEC 61158-6)
InOut:
Name |
Type |
Comment |
status1 |
IIoDrvProfibus.DP_StationStatus1 |
DP station status 1 |
status2 |
IIoDrvProfibus.DP_StationStatus2 |
DP station status 2 |
status3 |
IIoDrvProfibus.DP_StationStatus3 |
DP station status 3 |
Diag_Master_Add |
USINT |
address of the DP-master (Class 1) which has parameterised this DP-slave (255 means invalid or no parameterisation). |
Ident_Number |
UINT |
Ident Number of DP slave |
ExtDiag |
ARRAY [0..235] OF BYTE |
Extended Diagnosis Data |