TYPE ErrorCode :
The STATUS output has the data type DWORD which is interpreted as a packed array of four bytes.
Byte 0: Function_Num
Byte 1: Error_Decode
Byte 2: Error_Code_1
Byte 3: Error_Code_2
The Elements are used as specified in IEC 61158-6 (Profibus DP, Profinet IO)
Exception: If Function_Num has a value of 16#40, no protocol element is used. This is the case for example if the validation of one input parameter failed. In this case Error_Decode value of 16#82..16#8F reports an error at parameter number 2 - 15.
Other fixed error codes are defined in this enum.
InOut:
|
Name |
Initial |
Comment |
|
0 |
No error |
|
|
16#40000100 |
Unknown error |
|
|
16#40000101 |
Function not implemented |
|
|
16#40000102 |
tried to use RDIAG on Profinet device |
|
|
16#40000103 |
Stack not running. |
|
|
16#40000104 |
Out of ressources or ressource busy. |
|
|
16#40000105 |
specified local data-buffer size too small |
|
|
16#40000110 |
requested operation not possible in this state |
|
|
16#40000111 |
target-address is not unique |
|
|
16#40000112 |
address is invalid or unreachable (e.g. different IP subnet) |
|
|
16#40000113 |
unable to detect/address target-device |
|
|
16#40000114 |
target device has wrong type for requested operation |
|
|
16#40000115 |
Operation timed out |