FUNCTION ID : DWORD
This function converts the physical identification of a slot or a DP-slave to a handle which can be used with Communication Function Blocks.
InOut:
Scope |
Name |
Type |
Initial |
Comment |
Return |
ID |
DWORD |
||
Input |
EN |
BOOL |
TRUE |
|
MASTER |
BYTE |
ID of the DP system |
||
SEGMENT |
BYTE |
Number of the DP segment |
||
STATION |
BYTE |
Number of the DP-slave(station address) |
||
SLOT |
BYTE |
Slot number |