FUNCTION_BLOCK ID_TO_ADDR
The function block ID_TO_ADDR converts the handle used for the Communication Function Blocks to the physical identification of a slot of a PROFIBUS DP-slave or subslot of a PROFINET IO Device.
Code-Example: see RALARM
InOut:
Scope |
Name |
Type |
Initial |
Comment |
Input |
EN |
BOOL |
TRUE |
Enable |
ID |
DWORD |
Slot or subslot handle |
||
Output |
ENO |
BOOL |
Flag |
|
STATUS |
DWORD |
Last detected status |
||
Inout |
ADDR |
Physical address information |