TYPE PRVREC_MODE :
InOut:
|
Name |
Initial |
Comment |
|
0 |
If the Field Device interface has received a request to provide a process data record, only the outputs NEW, SLOT, INDEX and RLEN are set. Multiple calls of this function block with MODE=0 returns the outputs for the same request. |
|
|
1 |
If the Field Device interface has received a request, the function block outputs are updated. |
|
|
2 |
If the Field Device interface has received a request for the slot and subslot the numbers of which are given in F_ID input, the function block outputs are updated. |
|
|
3 |
After checking or receiving the request to provide a process data record, this function block provides the requested process data record with its RECORD parameter and sends a positive response to the Host Controller. |
|
|
4 |
After checking or receiving the request to provide a process data record, this function block refuses to provide this record and sends a negative response to the Host Controller. The error reason is given with the inputs CODE1 and CODE2. |