TYPE RALARM_MODE :
Filter scope of RALARM.F_ID input.
InOut:
Name |
Initial |
Comment |
1 |
If the Host Controller interface has received an alarm, all function block outputs are updated. The alarm is acknowledged. |
|
2 |
Receive an alarm for the slot or subslot the identification of which is given in F_ID input, all function block outputs are updated. The alarm is acknowledged |
|
3 |
Receive an alarm for the slot the identification of which is given in F_ID input AND for all of it's subslots |
|
4 |
Receive an alarm for the device the identification of which is given in F_ID input AND for all of it's slots and subslots |