TYPE RCVREC_MODE :
InOut:
|
Name |
Initial |
Comment |
|
0 |
If the Field Device interface has received a process data record, only the outputs NEW, SLOT, INDEX and RLEN are set. Multiple calls of this function block with MODE=0 returns the outputs for the same request. |
|
|
1 |
If the Field Device interface has received a process data record, the function block outputs are updated and the data record is transferred to the RECORD parameter. |
|
|
2 |
If the Field Device interface has received a process data record for the slot or subslot the num-bers of which are given in input F_ID, the function block outputs are updated and the data re-cord is transferred to the RECORD parameter. |
|
|
3 |
The service is responded positively. |
|
|
4 |
After checking the request to receive a process data record, this function block refuses to accept this record and sends a negative response to the Host Controller. The error reason is given with the inputs CODE1 and CODE2. |