SETIO_PART (FB)

 

FUNCTION_BLOCK SETIO_PART

The SETIO_PART function block sets the output data for a subset of the output data associated to a slot or subslot of a Field Device. The output data are addressed within the slot or subslot through the OFFSET and LEN parameters. The SETIO_PART function block sets the output data to the Host Controller interface into the cyclically written output data of the Field Device. The function block is invoked by a 1 of the EN input. If the Output data are stored successfully and the Field Device is still cycli­cally communicating, the ENO output is set to 1.

If the Output data are stored successfully and the Field Device is still cyclically communicating, the ENO output is set to 1

Never use GETIO-/SETIO_PART FBs concurrently with %I/%Q-Input/Output-Mapping for the same slot/subslot !

InOut:

Scope

Name

Type

Comment

Input

EN

BOOL

Enable

ID

DWORD

Identifier of a slot / subslot of a Field Device

OFFSET

INT

Offset of the subset of output data

LEN

INT

Length of the output data to write

OUTPUTS

POINTER TO BYTE

IO data object to write

Output

ENO

BOOL

Flag indication sending data OK

STATUS

DWORD

Last detected status

ERROR

BOOL

Flag indication an error