FUNCTION_BLOCK Apply_Attributes EXTENDS BaseService
This function block is used for calling the "Apply_Attributes" service of a specific instance of a CIP object. As a result, the attributes that were previously set with "Get_Attribut_Single" or "Get_Attribut_All" are adopted and saved by the adapter.
InOut:
Scope |
Name |
Type |
Comment |
Inherited from |
Input |
itfEtherNetIPDevice |
IEtherNetIPService |
EtherNet/IP Device which implements the EtherNet/IP Services interface |
BaseService |
eClass |
Class which shall perform the service |
BaseService |
||
dwInstance |
DWORD |
Instance which shall perform the service (0: Class level, 1..x: Instance level) |
BaseService |
|
Output |
eError |
Error (0-255: CIP Error; 256-x: Library Error) |
BaseService |