CIPCommonService (ENUM)

 

TYPE CIPCommonService :

CIP Service Codes and Names

InOut:

Name

Initial

Comment

None

16#0

GET_ATTRIBUTES_ALL

16#1

SET_ATTRIBUTES_ALL

16#2

RESET

16#5

START

16#6

STOP

16#7

APPLY_ATTRIBUTES

16#D

GET_ATTRIBUTE_SINGLE

16#E

SET_ATTRIBUTE_SINGLE

16#10

NO_OPERATION

16#17