FUNCTION_BLOCK Generic_Service EXTENDS BaseService
This function block performs a generic service at an EtherNet/IP Adapter. The message will be sent as an unconnected explicit message request.
Note
Data received and send needs to be swapped. See parent folder.
/// Force trigger to TRUE to activate.
/// Example device used here is WAGO 750-352 FC ETHERNET.
/// But you can adapt it, by using the services which are implemented by your prefered device.
PROGRAM PLC_PRG
VAR
dut : ENIP.Generic_Service ;
data: usint:=16#FF;
trigger: BOOL;
END_VAR
dut.xExecute := trigger;
dut.itfEtherNetIPDevice := WAGO_750_352_FC_ETHERNET;
dut.eClass := 100;
dut.dwInstance := 1;
dut.wAttribute := 11;
dut.eService := ENIP.CIPCommonService.SET_ATTRIBUTE_SINGLE;
dut.pWriteData := ADR(data);
dut.udiWriteDataSize := 1;
dut();
InOut:
|
Scope |
Name |
Type |
Comment |
Inherited from |
|
Input |
itfEtherNetIPDevice |
IEtherNetIPService |
EtherNet/IP Device which implements the EtherNet/IP Services interface |
BaseService |
|
eClass |
Class which shall perform the service |
BaseService |
||
|
dwInstance |
DWORD |
Instance which shall perform the service (0: Class level, 1..x: Instance level) |
BaseService |
|
|
Output |
eError |
Error (0-255: CIP Error; 256-x: Library Error) |
BaseService |
|
|
Input |
wAttribute |
WORD |
Attribute the services is addressed to. Leave 0 if this service does not address an attribute. |
|
|
eService |
Choose one of the CIPCommonService members, or insert any vendor specific service code. |
|||
|
pWriteData |
POINTER TO BYTE |
Data to write to the EtherNet/IP Adapter. Leave 0 if no data should be sent to the EtherNet/IP Adapter. |
||
|
udiWriteDataSize |
UDINT |
Size of data to write to the EtherNet/IP Adapter. Leave 0 if no data should be sent to the EtherNet/IP Adapter. |
||
|
pReadData |
POINTER TO BYTE |
Data expected to receive from the EtherNet/IP Adapter. Leave 0 if no data is expected to be received from the EtherNet/IP Adapter. |
||
|
udiReadDataSize |
UDINT |
Size of data expected to receive from the EtherNet/IP Adapter. Leave 0 if no data is expected to be received from the EtherNet/IP Adapter. |
||
|
Output |
udiReceivedDataSize |
UDINT |
Size of the received data |