Start (FB)

 

FUNCTION_BLOCK Start EXTENDS BaseService

This function block is used for calling the "Start" service of a specific instance of a CIP object. The exact effect of this service depends on the CIP class (refer to the CIP specifications (Vol. 1 and 2).

InOut:

Scope

Name

Type

Comment

Inherited from

Input

itfEtherNetIPDevice

IEtherNetIPService

EtherNet/IP Device which implements the EtherNet/IP Services interface

BaseService

eClass

CIPClass

Class which shall perform the service

BaseService

dwInstance

DWORD

Instance which shall perform the service (0: Class level, 1..x: Instance level)

BaseService

Output

eError

ERROR

Error (0-255: CIP Error; 256-x: Library Error)

BaseService