Example Description

 

Overview

Short Description

This document describes an application example for implementing read and write access to a file in CSV format using the function blocks from the FileFormatUtility library.

System Requirements and Limitations

The application example has been created with the components listed in the table:

Component

Type and Version

Software

oEcoStruxure Machine Expert V1.1

Controller

oModicon M251 Logic Controller

NOTE: The concepts presented in the application example are, in principle, transferable to other controllers supporting the controller firmware released in conjunction with EcoStruxure Machine Expert V1.1.