Safety Module Parameters and Process Data Items

 

The parameters of the safety-related modules can be set in the safety-related Device Parameterization Editor. This editor is part of the EcoStruxure Machine Expert - Safety 'Devices' window.

To edit the parameters of a safety-related module, left-click the respec­tive tree node in the 'Devices' window. Its parameters are then visible in the grid tabs on the right.

Further Information

For further information refer to the "Device Parameterization" topic of the EcoStruxure Machine Expert - Safety docu­mentation.

The process data items are listed under the module node in the device tree. These signals can either be read or written by the application (depending on the signal type). When dragging a process data item from the 'Devices' window into the safety-related code, a global variable is created.

Further Information

Also refer to the topic "Connecting/Disconnecting Process Data Items and Global I/O Variables" in the EcoStruxure Machine Expert - Safety online help.

Further Information

Refer to the respective device manual for further safety-related information and parameter-/module-specific hazard messages.

Safety-Related Products of the Safety Logic Controller system

The Safety Logic Controller system is comprised of the following safety-related products:

Module Type

Reference

Safety Logic Controller, SLC 100 Sercos III, 24 VDC

TM5CSLC100FS

Safety Logic Controller, SLC 200 Sercos III, 24 VDC

TM5CSLC200FS

Safety-related Module 2DI 24 VDC

TM5SDI2DFS

Safety-related Module 4DI 24 VDC

TM5SDI4DFS

Safety-related Module 20DI 24 VDC

TM5SDI20DFS

Safety-related Module 2DO 24 VDC, 0.5 A

TM5SDO2TFS

Safety-related Module 2DO 24 VDC, 2 A

TM5SDO2TAFS

Safety-related Module 2 relay outputs 24 VDC, 6 A

TM5SDO2DTRFS

Safety-related Module 4DO 24 VDC, 0.5 A

TM5SDO4TFS

Safety-related Module 4DO 24 VDC, 2 A

TM5SDO4TAFS

Safety-related Module 6DO 24 VDC, 0.2 A

TM5SDO6TBFS

Safety-related Module 2DI (2 pulse output), 2DO 24 VDC, 6 A

TM5SDM4DTRFS

Safety-related Module 6DI (6 pulse output), 6DO 24 VDC, 0.5 A

TM5SDM8TBFS

IP67 Block, 8DI, 4DO, 2 A

TM7SDM12DTFS

Safety-related Module 8DI (2 standard DI, 2 pulse output), 2standard DO 24 VDC, 12 A, M12 device interface

TM7SDI8DFS

Safety-related Module 4AI (2x2 current input, 4 to 20 mA, 24 bit converter resolution)

TM5SAI4AFS

Safety-related Temperature Module (2x2 analog thermocouple inputs for thermoelements of the types J, K, N, S, R, C, T and 1x2 safety-related analog PT100/PT1000 input, 24 bit converter resolution)

TM5STI4ATCFS

Safety-related Digital Counter Module (1 safety-related digital counter channel, max. input frequency 7 kHz, 24 VDC)

TM5SDC1FS

Safety-related Power Supply Module (24 VDC, 10 A)

TM5SPS10FS

Safety Module for LXM62 Drives

LXM62FS

Safety Module for ILM62 Drives

ILM62FS

TM5 Bus Base for safety-related Electronic modules, safety coded, internal I/O supply interconnected

TM5ACBM3FS

Safety-related Terminal Block, 12-pin, safety coded

TM5ACTB52FS

Memory Key 2 MB1

TM5ACSLCM2FS

Memory Key 8 MB1

TM5ACSLCM8FS

1

A memory key is required for operation of the Safety Logic Controller. For more information concerning the role of the memory key in the Safety Logic Controller system, refer to the Safety Logic Controller SLC100/200 FS - Hardware Guide.

Only modules designated as safety-related modules are allowed to perform safety-related functions. Make certain that neither inputs nor outputs of non-interfering modules are used for safety-related inputs or outputs.

DANGER

IMPROPERLY CONFIGURED SAFETY-RELATED SYSTEM

  • Use only products designated as functional safety devices for use in a safety-related system.

  • Use only Schneider Electric authorized products in a Safety Logic Controller system.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

NOTE:

The Sercos III Bus Interface, required for communication with safety-related TM5 modules, is considered a non-inter­fering module and does not contribute nor detract from the safety-related function of the controller. The safety support layer riding on the Sercos III communication is managed inside the safety-related modules and not in the Sercos III Bus Interface.

Example: Parameters and process data items of a digital input safety-related module

After selecting a module in the Devices tree on the left, the parameters are visible and can be edited in the grids on the right. The process data items (signals) of a module can be dragged into FBD/LD code work­sheets thus creating a related global variable which can be read or written by the application (depending on the signal type).

SoSafe_HWParameter.png