Aliases

 

Aliases

Overview

Type:

ALIAS (DUT)

Available as of:

V1.0.0.0

Inherits from:

Description

An alias represents a complex data type which is used in this library.

TlsSettings

Name

Data type

Description

TlsSettings

TcpUdp.ST_TlsSettingsClient

Specifies the TLS (Transport Layer Security) settings for the secured connection to be established.

Refer to TcpUdp.ST_TlsSettingsClient.