|
Step |
Action |
|---|---|
|
1 |
Download the MachineExpertInstaller-*-Setup.exe file from the Schneider Electric website at https://www.schneider-electric.com/en/product-range-download/2226-ecostruxure%E2%84%A2-machine-expert#tabs-top. |
|
2 |
Double-click the MachineExpertInstaller-*-Setup.exe to install the Machine Expert Installer on your Windows system. Result: The Windows User Account Control dialog box is displayed. |
|
3 |
Confirm the User Account Control by clicking the Yes button. NOTE: If the software is already installed, you are prompted to either remove the existing installation or to repair the existing installation. |
|
4 |
In the Choose Setup Language dialog box, select the language for this installation procedure from the list and click the OK button. |
|
5 |
In the Welcome to the Installation Wizard for Machine Expert Installer dialog box, click the Next button. Result: The License Agreement dialog box is displayed. |
|
6 |
Read the License Agreement and if you so choose, select the option I accept the terms of the license and click Next to start the installation. Result: After the installation has been completed successfully, the window closes automatically and Machine Expert Installer is started. |
|
7 |
In the Ready to Install the Program dialog box, click the Install button to start the installation. |
|
8 |
When the Installation Complete dialog box is displayed, click the Finish button to terminate the installation. Result: The program starts automatically. |
After the installation, you can find the files of the Machine Expert Installer under one of the following paths:
oC:\Program Files (x86)\Schneider Electric\Machine Expert Installer
oC:\Program Files \Schneider Electric\Machine Expert Installer
To start the Machine Expert Installer manually when it is installed:
oDouble-click the Machine Expert Installer shortcut or
oRun the Machine Expert Installer from the Windows Start menu.
After starting the Machine Expert Installer, confirm the User Account Control by clicking the Yes button.
Starting the Installer via Windows Command Line
You can start the Machine Expert Installer via the Windows command line by executing the following command:
"C:\Program Files (x86)\Schneider Electric\Machine Expert Installer\MachineExpertInstaller.Cli.exe" Install-Product --productId=ESME
For further information, refer to the command line help of the Installer:
"C:\Program Files (x86)\Schneider Electric\Machine Expert Installer\MachineExpertInstaller.Cli.exe" --help