ERROR (ENUM)

 

TYPE ERROR :

CIP Error Codes from 1 - 16#69 and IoDrvEtherNetIP Error Codes from 16#AA-XX

InOut:

Name

Initial

Comment

NO_ERROR

0

INVALID_COMMAND

16#1

OUT_OF_MEMORY

16#2

INVALID_DATA

16#3

INVALID_SESSION_HANDLE

16#64

INVALID_LENGTH

16#65

UNSUPPORTED_PROTOCOL_VERSION

16#69

NBS_ERROR

16#AA

NBS_RCV_ERROR

NBS_SND_ERROR

ENCAPSULATION_ERROR

TCPIP_CONFIG_ERROR

UDP_CONFIG_ERROR

UDP_RECV_ERROR

UDP_SEND_ERROR

UDP_CLOSE_ERROR

NULL_POINTER

DEVICE_STATE_ERROR

RECONFIGURATION_FAILED

PERFORMANCE_MONITOR_DISABLED

INVALID_MEASURING_POINT

IP_CONFIG_ERROR