FUNCTION_BLOCK IoDrvEtherNetIP EXTENDS IoDrvBase IMPLEMENTS ICmpIoDrvParameter, IScanner, IoDrvEtherNetIPAdapter.IScannerExtension, CmpEventMgr.ICmpEventCallback
Driver FB: Don´t create this FB directly.
InOut:
Scope |
Name |
Type |
Comment |
Input |
xReset |
BOOL |
Rising edge to reset the scanner. |
Output |
eState |
State of the EtherNet/IP Scanner see ScannerState |
|
eError |
Specifies the error, if scanner is in error state see ERROR |