IoDrvEtherNetIP_diag (FB)

 

FUNCTION_BLOCK IoDrvEtherNetIP_diag EXTENDS IoDrvEtherNetIP IMPLEMENTS DED.IBus, DED.IStack, DED.IReconfigureProvider

Driver FB: Don´t create this FB directly.

InOut:

Scope

Name

Type

Comment

Inherited from

Input

xReset

BOOL

Rising edge to reset the scanner.

IoDrvEtherNetIP

Output

eState

ScannerState

State of the EtherNet/IP Scanner see ScannerState

IoDrvEtherNetIP

eError

ERROR

Specifies the error, if scanner is in error state see ERROR

IoDrvEtherNetIP