FUNCTION_BLOCK RemoteAdapter EXTENDS LAT.Element IMPLEMENTS CmpEventMgr.ICmpEventCallback, IRemoteAdapter2, ENIP.IEtherNetIPService3
Every device under the scanner is type of RemoteAdapter. Driver FB: Don´t create this FB directly.
InOut:
Scope |
Name |
Type |
Comment |
Input |
xReset |
BOOL |
Rising Edge: Reset this RemoteAdapter instance. Note: Device will not be reset (may be done through the ENIP Services library) |
xAcknowledge |
BOOL |
Rising Edge: Acknowledge diagnosis information --> xDiagnosticAvailable and sDiagString will be reset |
|
Output |
eState |
State of the RemoteAdapter |
|
xDiagnosticAvailable |
BOOL |
TRUE if diagnostics is available |
|
sDiagString |
STRING |
Diagnosis string - also shown in status page of the device |