RemoteAdapter_diag (FB)

 

FUNCTION_BLOCK RemoteAdapter_diag EXTENDS RemoteAdapter IMPLEMENTS DED.IDevice2

Driver FB: Don´t create this FB directly.

InOut:

Scope

Name

Type

Comment

Inherited from

Input

xReset

BOOL

Rising Edge: Reset this RemoteAdapter instance. Note: Device will not be reset (may be done through the ENIP Services library)

RemoteAdapter

xAcknowledge

BOOL

Rising Edge: Acknowledge diagnosis information --> xDiagnosticAvailable and sDiagString will be reset

RemoteAdapter

Output

eState

AdapterState

State of the RemoteAdapter

RemoteAdapter

xDiagnosticAvailable

BOOL

TRUE if diagnostics is available

RemoteAdapter

sDiagString

STRING

Diagnosis string - also shown in status page of the device

RemoteAdapter