TYPE ScannerState :
InOut:
|
Name |
Comment |
|
Setting up CIP objects. Go on with IP_CONFIG. |
|
|
Make ip configuration to ethernet interface and waiting for it to go on state IoDrvEthernet->EthernetState->RUNNING. Go on with UDP_CONFIG if ok. If error eState is ScannerState.ERROR and Error.TCPIP_CONFIG_ERROR. |
|
|
Open UDP default port 2222 socket for IO communication. If ok go on with UDP_CONFIG, else ScannerState.BUS_ERROR. |
|
|
Start the encapsulation server of the scanner on default port 44818 TCP. Go on with ADAPTER_CONFIG if ok, else ScannerState.BUS_ERROR. |
|
|
Empty state. Go on with OPEN_CONNECTIONS. |
|
|
Setting CIP identity status to configured and go on with state RUNNING. |
|
|
Open connections to adapters and handel IO communication and explicit messages (different tasks) |
|
|
Same as running with diagnostic message for configurator/editor. |
|
|
UDP or TCP ports could not be opened. If network interface is going on state IoDrvEthernet->EthernetState->RUNNING scanner jumps to state INITIALIZING. |
|
|
If xReset on CIP identity object is received this state is getting aktiv. |
|
|
If network interface is going on state IoDrvEthernet->EthernetState->RUNNING scanner jumps to state INITIALIZING. |