FUNCTION_BLOCK AdapterDiagnosis
Gets the diag. info of the given IoDrvEtherNetIPAdapter.
InOut:
Scope |
Name |
Type |
Comment |
Input |
pEtherNetIPAdapter |
POINTER TO IoDrvEtherNetIPAdapter |
The IoDrvEtherNetIPAdapter from which the diag. info is needed. |
Output |
uiConnectedModules |
UINT |
Number of modules connected at the adapter |
uiEstablishedClass1Connections |
UINT |
Number of currently successfull established connections |
|
udiConnectionTimeouts |
UDINT |
Number of connection timeouts since the adapter started |
|
udiForwardOpenRequests |
UDINT |
Total number of forward open requests processed by the adapter |
|
udiForwardOpenFails |
UDINT |
Number of unsuccessfull forward open requests |