TYPE ADAPTERSTATE :
An output of IoDrvEtherNetIPAdapter.
InOut:
Name |
Initial |
Comment |
0 |
Startphase |
|
1 |
Loading parameters |
|
2 |
Disabled in device tree |
|
3 |
Create CIP objects |
|
4 |
Configure TCP object and waiting for ethernet node |
|
5 |
Open ports UDP |
|
6 |
Open ports TCP |
|
12 |
Stack has started, but no scanner is connected |
|
7 |
Stack is running and scanner is connected |
|
8 |
Ethernet node is inactiv, waiting for ethernet node to come back (pull cable) |
|
9 |
Closing the connections opened in IMPLICITMESSAGING_CONFIG and EXPLICITMESSAGING_CONFIG |
|
10 |
This state is active, if a scanner registered this adapter as an extension for I/Os |
|
11 |
Fatal error: no license, no memory |
|
13 |
If the ethernet interface is not ready or available |