ERROR (ENUM)

 

TYPE ERROR :

An output of IoDrvEtherNetIPAdapter, which defines the ADAPTER­STATE.ERROR more precisely.

InOut:

Name

Comment

NO_ERROR

No error

TIME_OUT

St the moment unused

CONFIGURATION_FAILED

Initializing ressources, loading parameters of connector or interating over subconnectors (modules) failed

IP_CONFIG_FAILED

Ethernet node reported an error

IMPLICITMESSAGING_CONFIG_FAILED

Creating UDP port CIP_ENC.ParameterList.gc_uiUDPPort (default: 2222) failed

EXPLICITMESSAGING_CONFIG_FAILED

Creating TCP and UDP port IP_ENC.ParameterList.gc_uiTCPPort (default: 44818) failed

EXPLICITMESSAGE_RECEIVE_FAILED

Problem with sockets of TCP or UDP port |CIP_ENC.ParameterList.gc_uiTCPPort| (default: 44818)

EXPLICITMESSAGE_SEND_FAILED

Problem with sockets of TCP or UDP port |CIP_ENC.ParameterList.gc_uiTCPPort| (default: 44818)

LICENSE_MISSING

License is missing