FUNCTION_BLOCK IoDrvEtherNetIPAdapter EXTENDS IoDrvBase IMPLEMENTS IAdapter, CIP_Object.ICIPProvider
Is the FB generated from the device. To see which CIP objects are implemented download ENIP_Adapter_Objects.xls Driver FB: Don´t create this FB directly.
InOut:
Scope |
Name |
Type |
Comment |
Input |
xReset |
BOOL |
Rising Edge: Reset this IoDrvEtherNetIPAdapter instance. |
Output |
eState |
State of the EtherNet/IP Adapter see ADAPTERSTATE |
|
eError |
Specifies the error, if adapter is in error state see ERROR |