ReceiveParameterGroup (FB)

 

FUNCTION_BLOCK ReceiveParameterGroup EXTENDS CBM.ETrig IMPLEMENTS IReceiveParameterGroup

This function block represents a receive parameter group defined in J1939 configurator.

InOut:

Scope

Name

Type

Comment

Inherited from

Input

xExecute

BOOL

Rising edge: Action starts

Falling edge: Resets outputs

If a falling edge occurs before the func­tion block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.

ETrig

Output

xDone

BOOL

TRUE: Action successfully completed

ETrig

xBusy

BOOL

TRUE: Function block active

ETrig

xError

BOOL

TRUE: Error occurred, function block aborts action

FALSE: No error

ETrig

Input

itfECU

IJ1939ECU

ECU instance where parameter group belongs to.

dwPGN

DWORD

parameter group number

Output

itfParameterGroup

IReceiveParameterGroup

mainly for graphical programming: output for connection to other function blocks

eError

ERROR

detailed error information if xError is TRUE.