FUNCTION_BLOCK TransmissionTrigger EXTENDS CBM.ETrig
This function block triggers the transmission of a parameter group.
Note
The transmission is not done immediately. The function block only sets a flag in communication stack which causes a transmission in next bus cycle.
InOut:
|
Scope |
Name |
Type |
Comment |
Inherited from |
|
Input |
xExecute |
BOOL |
Rising edge: Action starts Falling edge: Resets outputs If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle. |
ETrig |
|
Output |
xDone |
BOOL |
TRUE: Action successfully completed |
ETrig |
|
xBusy |
BOOL |
TRUE: Function block active |
ETrig |
|
|
xError |
BOOL |
TRUE: Error occurred, function block aborts action FALSE: No error |
ETrig |
|
|
Input |
itfParameterGroup |
ITransmitParameterGroup |
parameter group which should be transmitted. |
|
|
Output |
eError |
detailed error information if xError is TRUE. |