FUNCTION_BLOCK TransmitParameterGroup EXTENDS CBM.ETrig IMPLEMENTS ITransmitParameterGroup
This function block represents a transmit parameter group defined in J1939 configurator.
InOut:
Scope |
Name |
Type |
Comment |
Inherited from |
Input |
xExecute |
BOOL |
Rising edge: Action starts Falling edge: Resets outputs If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle. |
ETrig |
Output |
xDone |
BOOL |
TRUE: Action successfully completed |
ETrig |
xBusy |
BOOL |
TRUE: Function block active |
ETrig |
|
xError |
BOOL |
TRUE: Error occurred, function block aborts action FALSE: No error |
ETrig |
|
Input |
itfECU |
IJ1939LocalECU |
ECU instance where parameter group belongs to. |
|
dwPGN |
DWORD |
parameter group number |
||
byDestinationAddress |
BYTE |
for P2P parameter groups: destination address; for broadcaste: do not care |
||
Output |
itfParameterGroup |
ITransmitParameterGroup |
mainly for graphical programming: output for connection to other function blocks |
|
eError |
detailed error information if xError is TRUE. |