FUNCTION_BLOCK PNSlaveDiag EXTENDS PNSlave IMPLEMENTS DED.IDevice2
see PNSlave
InOut:
Scope |
Name |
Type |
Initial |
Comment |
Inherited from |
Output |
xRunning |
BOOL |
Slave is in cyclic data exchange. |
||
xBusy |
BOOL |
Connect or abort currently in progress. |
|||
xError |
BOOL |
Communication error. Output PNIOStatus displays reason. |
|||
PNIOStatus |
UDINT |
16#FFFFFFFF |
The current PNIO Status of the device. |
||
xDiagnosis |
BOOL |
Any module of the slave has a diagnosis entry. |
|||
xModuleDiff |
BOOL |
The module configuration is not matching (wrong or missing). |