Dynamic Generation of FB Instances

In CODESYS there are two possibilities of dynamically creating an FB instance:

A.) By using the operators __NEW and __DELETE and a Memory­Pool which has to be parameterized for the respecting application via CODESYS.

However this method has a significant disadvantage:

  • The MemoryPool is defined once for the application and all the referenced libraries within the application. But it is not possible to determine how much storage space each library is allowed to claim in the MemoryPool.

  • The coincidental utilization of __NEW and __DELETE with different sized FB instances causes a fragmentation of the MemoryPool. Because of that it is not possible to securely install any system for a non-stop operation throughout the entire year. An occasional reboot of the facility would be necessary to re-establish the Memo­ryPool.

  • That is why the MemoryPool and the operators __New and __De­lete can only be recommended for applications in very special cases. Especially when dealing with libraries this method should not be used!

B.) By using the library FBFactory there is a second and more reli­able possibility to meet the demands of dynamically creating an FB instance.

With the help of the FBFactory Library a static pool (which can be extended into a dynamic pool if needed) for each factory is defined in advance. The management of the memory space is organized in way which makes sure that no fragmentation is possible. Therefore there is no obstacle to a non-stop operation of the system.

FBFactory Library can be used as a base for building factories. In order to get more information about how to use this library for building factories please download the Test Project which you will find in the documentation of the FBFactory Library

FBFactory_Docu.PNG

There you will find a Test Project which uses a Test Library that extends the FBFactoryLibrary. It is recommended to look at how the example program (PLC_PRG) works by setting a breakpoint and stepping into each action of the program. Do not go online in simulation mode! More­over the documentation of the FB Factory Test Library (which is already added to the Library Manager in the Test Project) explains what is done in each part of the library.

There is a template for libraries in CODESYS which is called CODESYS library which assists you building your own FB Factory. Therefore please open a new project and choose the category Libraries and afterwards the template CODESYS library.

1_NewProject_CODESYSLibrary.png

In this project the folder Templates contains the subfolder FBFactory with all the important FBs, Methods and Properties.

2_OrdnerFBFactory.png

All relevant Function Blocks should be copied in the folder with the title Function Blocks in order to be able to modify them.

Afterwards change the names of every element to suitable expressions.

3_OrdnerFunctionBlocks.png

By clicking on each element with the right mouse button and choosing Properties -> Build you can deactivate Exclude from build

4_ExcludeFromBuild.png

Moreover it is advisable to adapt the array abyPoolMemory in the func­tion block TestFBFactory to ones own needs.

5_TestFBFactory_Array.png

Make sure that everywhere in TestFBFactory (for exemple in the first line of the method TestFBFactory.Create) the expression Custom is substi­tuted by the name you chose for these elements.

6_TestFBFactory.Create.png

By calling up the method Create it is now possible to dynamically create a FB instance.