Templates

Rule #8:

Not from scratch - Use Templates (Optional)

Templates.png

Template Types

With each CODESYS version a set of templates is provided, which are a good basis for setting up libraries following the guidelines described here.

The recommended project structure is provided, and templates for the usage of an unique command interface for function blocks are available.

Function Blocks Design Patterns

One important part of this templates is a helpful collection of function blocks which implements different patterns of common behaviour models.