Visibility modifiers also none as access modifiers can be applied to some elements of CODESYS project or library. CODESYS will provide two groups of these modifiers.
Attributes for decorating POU's
Attributes will control the visibility of some elements in a way that a user of CODESYS will not able to see this element. The CODESYS compiler is still able to use these elements. An application which is using a element decorated with one of these attributes will not present an compile error.
Special Keywords like PUBLIC, PROTECTED, INTERNAL, PRIVATE for decorating Programs, Function Blocks, Properties and Methods
With the help of these special keywords it is possible to define the access rights for a specific element. An application which is using a element decorated with one of these keywords will present an compile error if the access to this element is not allowed by the related keyword.
Attributes for Controlling the Visibility
In the CODESYS library template, concrete examples for the usage of some attributes regarding the visibility of symbols are provided:
{attribute 'qualified_only'} for enums types
This attribute introduces a new name space. So one member of a enum type can be reused in an other enum type.
For accessing a member of a enum type decorated with this attribute prefixing the name of this member
with the name of the enum type is necessary.
{attribute 'qualified_only'}
TYPE ERROR : (NO_ERROR, TIME_OUT); END_TYPE
eErrorID : ERROR;
eErrorID := ERROR.NO_ERROR;
{attribute 'qualified_only'} for global variable lists
This attribute introduces a new name space. So one member of the gvl can be reused in an other gvl.
For accessing a member of a global variable list decorated with this attribute prefixing the name of this member
with the name of the variable list is necessary.
{attribute 'qualified_only'}
VAR_GLOBAL CONSTANT
gc_iDummy : INT := 42; /// This is a dummy global constant variable
END_VAR
iMyVar := GVL.gc_iDummy;
{attribute 'hide_all_locals'} for function blocks
This attribute hide all local variables.
{attribute 'hide_all_locals'}
FUNCTION_BLOCK ETrigA_Temp EXTENDS CBML.ETrigA
VAR_INPUT
(* specific inputs *)
END_VAR
VAR_OUTPUT
eErrorID : ERROR;
(* specific outputs *)
END_VAR
VAR
(* specific vars *)
END_VAR
{attribute 'conditionalshow_all_locals' := 'SomeText'} or {attribute 'conditionalshow_all_locals'} for function blocks
This attribute hide all local variables if the related library is installed as *.compiled-library.
If the related library is available in the repository as a *.library the local variables are visible.
{attribute 'conditionalshow_all_locals' := 'SomeText'}
//{attribute 'conditionalshow_all_locals'}
FUNCTION_BLOCK LCon_Temp EXTENDS CBML.LCon
VAR_INPUT
(* specific inputs *)
END_VAR
VAR_OUTPUT
eErrorID : ERROR;
(* specific outputs *)
END_VAR
VAR
(* specific vars *)
END_VAR
{attribute 'conditionalshow' := 'SomeText'} or {attribute 'conditionalshow'} for function blocks
This attribute hide the whole function block if the related library is installed as *.compiled-library.
If the related library is available in the repository as a *.library the function block is visible.
// This is a container to carry init data from the Create methode of the factory
// to the prvInstInit methode of the new generated function block instance
{attribute 'conditionalshow' := 'SomeText'}
//{attribute 'conditionalshow'}
{attribute 'enable_dynamic_creation'}
FUNCTION_BLOCK CustomData EXTENDS FBF.InstanceData
VAR_INPUT
(* Todo: Add your application specific data as input variables *)
END_VAR
Decorating elements with the attributes {attribute 'hide_all_locals'} or {attribute 'hide'} are useful for securing the encapsulated knowledge. These attributes hiding the related elements without any condition. The related elements can not handled properly by CODESYS features like Refactoring or Cross Reference.
The elements decorated with {attribute 'conditional show_all locals' := 'SomeText'} or {attribute 'conditional show' := 'Some Text'} are hidden for the end user, but visible for the library developer.
Calling CODESYS with the command line parameter --conditionalshowsymbols="SomeText" activates the visibility of the special marked parts of a library for the end user.
Keywords for Controlling the Visibility
The main difference between controlling visibility with attributes to the method of using keywords is that these keywords will not simply hide symbols. The related symbols are really not accessible.
To encapsulate parts of your application has naturally some pros and cons.
Pros
Because the implementation of a function block is not known to other classes, the implementation can be modified without affecting collaboration with other function blocks.
Increased clarity as only the public interface of a class needs to be considered (Debugging, Documentation).
Cons
Unit testing a maximum encapsulated function block is not so easy, because the access to specific internals is not possible.
Note
In the future, solving CDS-51581 may provide a better way to handle such situations.
PUBLIC:
This is the default. If no access modifier or the keyword PUBLIC is used, no access limitation is defined.
PROTECTED:
Access is only allowed for the own members or members of function blocks which extends the current function block.
INTERNAL:
Access is only allowed for the members of the current library. Symbols which are decorated with this keyword are not accessible and not visible from outside of the library.
PRIVATE:
Access is only allowed for the own members of a function blocks.