|
Type: |
Enumeration |
|
Available as of: |
V1.0.0.0 |
|
Default value: |
E_Working |
The enumeration ET_TestReturn includes the states of the test. It is relevant for internal execution of the test.
|
Name |
Value |
Description |
|---|---|---|
|
0 |
Test case / test sequence is executed. |
|
|
1 |
Test case / test sequence completed successfully. |
|
|
2 |
Test case / test sequence not successful. |
ET_TestReturn is the datatype of the return value of IF_TestCase.