The PD_ETest library provides a collection of assistant function blocks for the ETEST framework of the Logic Builder. For further information on the ETEST framework and its use, refer to the ETEST User Guide.
When you create a test case in the Logic Builder, the PD_ETest library is automatically integrated in your project. You cannot use ETEST framework without this library.
NOTE: The PD_ETest library is only used in connection with the ETEST framework that is integrated in Logic Builder. The functions and function blocks contained in this library are used implicitly, and are not programmed in the user application.
The POUs of the PD_ETest library can only be accessed from test case objects and resource objects, which have been created in the ETEST framework.
If you attempt to use these functions and functions blocks directly in your application, it can lead to compile errors.