EcoStruxure Machine Expert version 1.1 does not support the M258, LMC058 and LMC078 controllers.

Appendices

Overview

This appendix provides examples for defining GVLs and GNVLs. It shows an example for exchanging network variables between applications of different programming system versions, and it gives general information on functions and function blocks.

What Is in This Appendix?

The appendix contains the following chapters:

oExample of a Simple Network Variable Exchange

oCompatibility

oFunction and Function Block Representation