Installation with Machine Expert Installer
The OPC server is available for installation with the Machine Expert Installer.
No OPC server icon is available in the Windows notification area. It is listed in the Windows Task Manager as a process.
Executing the OPC Client on a PC not Running EcoStruxure Machine Expert
To be able to execute the OPC client on a PC where EcoStruxure Machine Expert is not installed, proceed as follows:
oInstall the gateway component on the PC where the OPC client is running. Depending on the OPC client, you need to launch the WinCoDeSysOPC.exe file.
oCopy the file OPCServer.ini to the same directory where the WinCoDeSysOPC.exe is installed.